Issue:
Replacement HOA for 8539 NEMA 7/9 rated combo starter.
Product Line:
NEMA and Definite Purpose Contactors and Starters
Environment:
Type S combination starter accessories
Resolution:
Yes. The part number is 2949520507 for the operator. You must also use a 9001KA1 contact block for that three position switch.
Replacement HOA for 8539 NEMA 7/9 rated combo starter.
Product Line:
NEMA and Definite Purpose Contactors and Starters
Environment:
Type S combination starter accessories
Resolution:
Yes. The part number is 2949520507 for the operator. You must also use a 9001KA1 contact block for that three position switch.
Released for:Schneider Electric Canada