Search FAQs
Can the instantaneous function on Powerpact P, R, and Masterpact NT and NW be disabled?
Issue:
What are the Instantaneous override value for the Powerpact P, R and Masterpact?
Product Line:
Circuit Breaker
Resolution:
The instantaneous setting can be turned OFF if the breaker has the short time function (5.0 or 6.0 trip unit). BUT there is an instantaneous override function which will trip the breaker instantaneously on a high level fault. See attachment for override values.
What are the Instantaneous override value for the Powerpact P, R and Masterpact?
Product Line:
Circuit Breaker
Resolution:
The instantaneous setting can be turned OFF if the breaker has the short time function (5.0 or 6.0 trip unit). BUT there is an instantaneous override function which will trip the breaker instantaneously on a high level fault. See attachment for override values.
Released for:Schneider Electric Canada
Attachment(s)
Explore more
Range:
Explore more
Range: