{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the pretravel for the XCMB510 and XCMB502?
Issue:
Pretravel information on the XCMB limit switches

Product Line:
XCMB Limit Switches

Environment:
OsiSense XC Switches

Resolution:
The pretravel for the XCMB510 is 1.8mm and for the XCMB502 it is 3.1mm

Schneider Electric Canada

Explore more
Category:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Category: