{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Which handle comes standard with a VCF02, VCF01, VCF0, VCF1, or VCF2?
Issue:
What is the standard handle that comes with Tesys Vario VCF?

Product Line:
Operating Mechanisms and Disconnect Switches

Environment:
Tesys Vario

Resolution:
The Red/Yellow Four Hole 60 X 60 mm handle part number is KCF1PZ.

Schneider Electric Canada