{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How do you order an 8903 mechanically held contactor with form R6 (2 wire control) if the contactor coil and the R6 relay coil are to be two different voltages?
Issue:
Identify a part number for a 8903 Mechanically held contactor with R6 form that uses different coil voltage for the relay and the contactor.

Product Line:
NEMA 8903 Lighting Contactors

Environment:
NEMA Contactors and Starters

Cause:
Need to utilize different control voltages for the relay and the mechanically held contactor's coil

Resolution:
In the catalog part number, use a voltage code of V99 and then specify the R6 control voltage and contactor control voltage when ordering.

Schneider Electric Canada

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.