{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the part number for the replacement bulb for the Pilot Light supplied in a size 0, NEMA 7/9 enclosed contactor or starter?
Issue:
Identify a replacement bulb for NEMA 7/9 pilot lights

Product Line:
Class 8536 Contactors and Starters

Environment:
Square D NEMA Contactors and Starters

Resolution:
Since the cover-mounted units for the explosion proof starters are made by Curlee, the bulb would need to be obtained from them. The entire pilot light assembly can be purchased from Square D by ordering part number 29495-20209 but we cannot provide just the bulb.

Schneider Electric Canada

Explore more
Range:
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
Product: