{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the replacement starter in an enclosed 3-pole NEMA size M-0 manual motor starter for AC applications?
Issue:
Looking for the replacement starter in an enclosed 3-pole NEMA size M-0 manual motor starter for AC applications.

Product Line:
Type M Manual Starter

Environment:
NEMA Contactors and Starters

Resolution:
To replace only the starter, use the 2510MBO2 for the ones with the square push button operators or 2510TBO2 for the ones with the toggle operator.

Schneider Electric Canada

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.