{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the catalog number of replacement reset button for a NEMA size 0 or 1 combination starter in a NEMA type 1 or 12 oversized enclosure?
Issue:
Replacement reset button part # for a NEMA size 0 or 1 combination starter in a NEMA type 1 or 12 oversized enclosure

Product Line:
NEMA Starters

Environment:
NEMA Type S Motor Starters (8536 8736 8606)

Resolution:
The complete, door mounted, external reset mechanism assembly requires the following parts:

Qty 1 - 30019-113-64 Reset sub-assembly (does not include the ring nut, gasket or boot listed below).
Qty 1 - 30019-121-01 Ring nut.
Qty 1 - 29206-30700 Gasket (required on NEMA Type 12 enclosures).

Schneider Electric Canada