{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
On the EE30T6HCT, EE30T151HCT, and other CT Transformers which lead is the secondary center tap?
Issue:
Center Tap identification

Product Line:
LV Transformers

Environment:
Applies to Low Voltage Transformers from SquareD/Schneider Electric

Cause:
Secondaries of Transformers may have center taps

Resolution:

The secondary center tap is labelled X4. This applies to all step-down ``CT`` Transformers. The X4 terminal can be bonded to ground to meet NEC grounding requirements.

Schneider Electric Canada