{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Are Non-Ventilated Transformers available in stainless steel enclosures?
Issue:
Stainless Steel Transformer enclosures

Product Line:
LV Transformers

Environment:
Applies to Transformers by SquareD/Schneider Electric

Cause:
Stainless Steel Transformer enclosures  are often required

Resolution:
Yes! The Totally Enclosed Non-Ventilated (TENV) enclosures can be supplied in painted stainless steel, contact your local Field Office for a quote. SquareD/Schneider Electric also offers them in the Style A, B, and C resin encapsulated, Style E non-ventilated, and only stainless steel in a NEMA 4X offering.

Schneider Electric Canada