{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the replacement starter in an enclosed 3-pole NEMA size M-1 manual motor starter for AC applications?
Issue:
Checking on the replacement starter in an enclosed 3-pole NEMA size M-1 manual motor starter for AC applications.

Product Line:
NEMA Manual Starters and Switches

Environment:
NEMA Contactors and Starters

Resolution:
To replace only the starter, use the 2510MCO3 for the ones with the square push button operators or 2510TCO3 for the ones with the toggle operator.

Schneider Electric Canada