{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Are ANY of the EZM metering devices available with ALL copper bus?
Issue:
Product Design Features

Product Line:
EZ Metering Equipment

Resolution:
No. EZM metering, mains, and branch units are designed to meet UL67 standard, and are UL listed as modular panelboards. Bus bar sizes and material types are determined based on heat rise testing. Square D reserves the right to use either aluminum or copper current carrying conductors to comply with the UL standard.

NOTE:
Some of the EZM branch units are available with copper main horizontal cross bus, but this does not mean that ALL bussing within the device is copper.

Schneider Electric Canada

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.