{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the catalog number for a replacement non-compensated, bimetallic overload for a series A, Size 5 starter?
Issue:
Identifying available overload relay options

Product Line:
NEMA and Definite Purpose Contactors and Starters

Environment:
NEMA Bimetallic overloads

Resolution:
Non-compensated bimetal overload relays are no longer available in the NEMA product line. The replacement scenario was a 31102-084-50 CT assembly, a 9065SEO6B2 overload, and (3) 21926-28280 overload to contactor mounting screws. Select thermal units from table 38. As the bimetal overloads relays are now obsolete with no direct replacement, depending on the application we can use either of the following complete replacement assemblies: melting alloy overload relay 9065SEO5 or solid state overload relay 9065SF520.

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: