{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What are the instantaneous hold and trip ratings for EDB, EGB, and EJB breakers?

Issue:
What is the instantaneous rating for E-Frame Breakers?

Product Line:
Circuit Breakers

Resolution:
For 15 through 30 A, E Frame breakers:
Hold Rating: 270 A
Trip Rating: 875 A

For 35 through 70 A, E Frame breakers:
Hold Rating: 630 A
Trip Rating: 1800 A

For 80 through 125 A, E Frame breakers:
Hold Rating: 1000 A
Trip Rating: 2300 A

Schneider Electric Canada