{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Will the 9001K60 work with a 9001KR7U type operator?
Issue:
9001K60 padlock attachment compatibility with 9001 K operator

Product Line:
Push Buttons and Operator Interface

Environment:
Harmony 30 mm 9001 K/SK Push Buttons

Resolution:
Yes, 9001K60 is compatible with Type K and SK Operators.

Schneider Electric Canada