{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the part numbers of a cover for an unused space in a Model 4 LVMCC?
Issue:
Blank covers for Model 4 MCC?

Product Line:
Obsolete, Model 4 motor control centers.

Environment:
Products sold in North America.

Cause:
Maintenance

Resolution:
8998K401 - 1/2 Space Factor (6 inch) Blank Cover Plate
8998K402 - 1 Space Factor (12 inch ) Blank Cover Plate
8998K404 - 2 Space Factor (24 inch) Blank Cover Plate

Schneider Electric Canada

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.