{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the coil resistance of an 8501KP12V14 relay if it has a 24VAC coil?
Issue:
Coil resistance on the 8501K type relays

Product Line:
General Purpose Relays

Environment:
NEMA Industrial Relays

Resolution:
That relay has a coil resistance of 75 ohms at 20 degrees C.

Schneider Electric Canada