{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What are the replacement power terminal lugs for an 8502 or 8536 SF NEMA Size 4 contactor or starter?
Issue:
Lugs for 8502 or 8536 SF NEMA Size 4 contactor or starter.

Product Line:
Type S Full Voltage Contactors and Starters

Environment:
Starters, Type S

Resolution:
The lug assembly is part number 25050-34404.  Quantity of 6 for 3 poles.

Schneider Electric Canada