Search FAQs
Can an 8502 Type SD Size 2 contactor be used to replace the contactor in an 8536 Type SD Size 2 starter?
Issue:
Can I use an 8502 Type SD Size 2 contactor to replace the contactor in an 8536 Type SD Size 2 starter?
Product Line:
NEMA and Definite Purpose Contactors and Starters
Environment:
Class 8502/8536 Contactors and Starters Type SD
Resolution:
No. The load side on the 8502 contactor will not match up with line side of the overload relay.
Can I use an 8502 Type SD Size 2 contactor to replace the contactor in an 8536 Type SD Size 2 starter?
Product Line:
NEMA and Definite Purpose Contactors and Starters
Environment:
Class 8502/8536 Contactors and Starters Type SD
Resolution:
No. The load side on the 8502 contactor will not match up with line side of the overload relay.
Released for:Schneider Electric Canada
Explore more
Range:
Explore more
Range: