{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Are replacement parts and auxiliary accessories still available for the Class 8536 and Class 8736 pre-type S starters?
Issue:
Looking for replacement parts and auxiliary accessories still available for the Class 8536 and Class 8736 pre-type S starters?

Product Line:
NEMA and Definite Purpose Contractors and Starters

Environment:
Pre-Type S Contactors and Starters

Resolution:
Type A, AF, AR, AU, B, C, CC, DD & FB thermal units are utilized with the Type S devices and are still available.

Some 31012-400-** (Type A Series B size 00 only) and 1861-S1-****(Type B All Series size 0) control coils may and still be available as they are also used with some active timing relay devices.
** represent ending digits depending upon voltage required.

All other component parts, parts kits, coils, accessories, etc. are obsolete and no longer available.

If complete replacement device is required or desired, please use the Competitive Cross Reference tool link below.
https://tools.se.app/xref/v2/prod/index.html

Schneider Electric Canada

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.