Search FAQs
Are replacement parts and auxiliary accessories still available for the Class 8538 and Class 8738 pre-type S fusible combination starters?
Issue:
Replacement parts and auxiliary accessories still available for the Class 8538 and Class 8738 pre-type S fusible combination starters
Product Line:
NEMA Fusible Disconnect Switch Combination Starters
Environment:
Combination Starters & Pump Panels
Resolution:
Class 9999 Type R6 & R7 disconnect switch electrical interlooks along with Class 9999 Type S1, S2, S3, S4 and S5 fuse clip kits are still available.
Type A, AF, AR, AU, B, C, CC, DD & FB thermal units are utilized with the Type S devices and are still available.
Some 31012-400-** (Type A Series B size 00 only) and 1861-S1-****(Type B All Series size 0) control coils may and still be available as they are also used with some active timing relay devices.
** & **** represent ending digest depending upon voltage required.
All other component parts, parts kits, coils, accessories, etc. are obsolete and no longer available.
If complete replacement device is required or desired, please use the Competitive Cross Reference tool link below.
Replacement parts and auxiliary accessories still available for the Class 8538 and Class 8738 pre-type S fusible combination starters
Product Line:
NEMA Fusible Disconnect Switch Combination Starters
Environment:
Combination Starters & Pump Panels
Resolution:
Class 9999 Type R6 & R7 disconnect switch electrical interlooks along with Class 9999 Type S1, S2, S3, S4 and S5 fuse clip kits are still available.
Type A, AF, AR, AU, B, C, CC, DD & FB thermal units are utilized with the Type S devices and are still available.
Some 31012-400-** (Type A Series B size 00 only) and 1861-S1-****(Type B All Series size 0) control coils may and still be available as they are also used with some active timing relay devices.
** & **** represent ending digest depending upon voltage required.
All other component parts, parts kits, coils, accessories, etc. are obsolete and no longer available.
If complete replacement device is required or desired, please use the Competitive Cross Reference tool link below.
Released for:Schneider Electric Canada
Explore more
Range:
Explore more
Range: