{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
Will other manufacturers' branch circuit breakers work in Square D QO or Homeline load centers?
Issue:
Product design Features

Product Line:
QO and Homeline Load centers

Resolution:
The Square D QO and Homeline load centers are UL tested, listed, and labeled to accept ONLY Square D circuit breakers.
NOTE: The use of any other manufacturers' breakers, will VOID the UL listing and warranty of the product.

QO and Homeline load centers are also designed and tested by Square D to performance levels which exceed Underwriters Laboratories Standards. Use of Other manufacturers breakers, other than Square D Circuit Breakers, May Adversely Affect User Safety and Impair Reliability. Square D disclaims all liability for damage, injury or non-performance caused by the use or failure of non-Square D circuit breakers.

Schneider Electric Canada

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: