{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Can a QOB3125VH or QOB3150VH be installed into an older style NQOB panelboard?

Issue:
Can a QOB3125VH or QOB3150VH be installed into an older style NQOB panelboard?

Product Line:
Panelboards

Environment:
NQOB, QOB breakers

Cause:
Product compatibility

Resolution:
No, these circuit breakers have not been tested or UL listed for use in the panelboard. The highest ampere rating for a three pole branch breaker for this panelboard is 100A.

Schneider Electric Canada

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: