Issue:
Temperature rise suffixes on Low Voltage Transformers
Product Line:
LV Transformers
Environment:
Products sold in North America
Cause:
Low Voltage Transformers have different insulation systems and temperature rise classifications
Resolution:
1. An F Suffix designates Class 180 insulation system with 115 deg C average temperature rise in the windings
2. An FB Suffix designates Class 180 insulation system with 80 deg C average temperature rise in the windings
3. An H Suffix designates Class 220 insulation system with 150 deg C average temperature rise in the windings
4. An HF suffix designates Class 220 insulation system with 115 deg C average temperature rise in the windings.
5. An HB suffix designates Class 220 insulation system with 80 deg C average temperature rise in the windings.
Insulation system is also often referred to as Insulation Class.
Released for:Schneider Electric Canada
Issue:
Temperature rise suffixes on Low Voltage Transformers
Product Line:
LV Transformers
Environment:
Products sold in North America
Cause:
Low Voltage Transformers have different insulation systems and temperature rise classifications
Resolution:
1. An F Suffix designates Class 180 insulation system with 115 deg C average temperature rise in the windings
2. An FB Suffix designates Class 180 insulation system with 80 deg C average temperature rise in the windings
3. An H Suffix designates Class 220 insulation system with 150 deg C average temperature rise in the windings
4. An HF suffix designates Class 220 insulation system with 115 deg C average temperature rise in the windings.
5. An HB suffix designates Class 220 insulation system with 80 deg C average temperature rise in the windings.
Insulation system is also often referred to as Insulation Class.
Released for:Schneider Electric Canada