{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What should be used as the insulating material between breaker terminals and the metal of an enclosure?

Issue:
What type of material can be used as a fiber insulation plate?

Product Line:
Molded Case Circuit Breakers

Resolution:
An electrical grade fiber such as Nomex is recommended.

Schneider Electric Canada