{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What are the jumpers available for an AB1ET435U ?
Issue:
AB1ET435U  Jumpers offered

Product line:
Terminal blocks

Environmnent:
Type AB1 Terminal blocks

Resolution:
We have 2 top center jumpers with screws AB1BE2 (2 pole ) or AB1BE (70 pole), 2 upper terminal comb style jumpers AB1CC42SUPRO (2 pole ) or AB1CC46SUPRO (6 pole), and 2 lower terminal comb style jumpers AB1CC42INFRO (2 pole) or AB1CC46INFRO (6 pole).

Schneider Electric Canada

Explore more
Category:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Category: