{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the handle padlock attachment for an LC, LE, LI, LX, or LXI circuit breaker?
Product Line:
Circuit Breakers

Resolution:
There is a padlock attachment that will allow the breaker to be locked in either the ON or OFF position. It is part number AHPALI, and it can be installed on existing breakers. When locked in the ON position, the breaker will still trip. Note that the padlock itself is not a part of this kit, and must be purchased separately. Use a padlock with shackle diameter of 3/16" to 3/8" (4.7mm to 9.5mm). Installation instructions attached.

Schneider Electric Canada

Attachment(s)
48040-920-03.pdf [288.6 KB]