{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the size of the terminal screws on the standard terminal block of a 9070 Type T and TF Industrial Control Transformer?

Issue:
T and TF style Industrial Control Transformers have terminal screws on the primary and secondary sides for external connections

Product Line:
LV Transformers

Environment:
Applies to Industrial Control Transformers by SquareD/Schneider Electric

Cause:
T and TF Industrial Control Transformers typically have 4 terminal screws on the primary side and 4 terminal screws on the secondary side

Resolution:

The terminal screws on the T and TF Industrial Control Transformers are an 8-32 x 3/8``size.



CTA-ID : 2018771

Schneider Electric Canada