{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What will cause a Motor Logic Solid State Overload Relay to trip out "prematurely" when using it with a variable frequency drive?

Issue:
Why are solid state overload relays incompatible with VFDs and VSDs?

Product Line:
9065 Motor Logic Overload Relays

Environment:
Products sold in North America

Resolution:
There can also be harmonics issues when using it with a VFD, whether it's wired into the input or output of the drive.

Schneider Electric Canada