{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the maximum QO, 3-pole, Plug-On breaker that can be used with the QO3100BNS, QO3100BNF and QO3100BNRB circuit breaker enclosures?
Issue:
Product design features

Product Line:
QO circuit breaker enclosures

Environment:
QO plug-on Circuit Breaker

Cause:
Application

Resolution:
The maximum QO, Plug-ON breaker that can be installed in these enclosures is 100amp MAX. These enclosures are 3phase(or 3pole), 240Vac Max., 100amp Max. with a solid neutral.
NOTE: These enclosures CANNOT be used with 1-Pole QO breakers.

Schneider Electric Canada

Explore more
Product:
Range:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
Range: