Issue:
Are Tesys F LC1F Contactors UL and CSA approved?
Product Line:
IEC Contactors and Starters
Environment:
TeSys F Contactors
Resolution:
Yes, for AC loads only. The UL File number is E164862 NLDX; the CSA Listing number is LR 43364, 3211 04.
Are Tesys F LC1F Contactors UL and CSA approved?
Product Line:
IEC Contactors and Starters
Environment:
TeSys F Contactors
Resolution:
Yes, for AC loads only. The UL File number is E164862 NLDX; the CSA Listing number is LR 43364, 3211 04.
Released for:Schneider Electric Canada