{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What are the part numbers for the replacement contact block assemblies and terminal block wiring receptacles for the 9001BR control stations?
Issue:
Identify the replacement parts for 9001BR control stations.

Product Line:
30mm Control Stations

Environment:
Push Buttons and Operator Interface

Cause:
Part number is trying to be identified for application.

Resolution:
Control Station      Contact Block     Assemblies Wiring Receptacle
BR101 - BR107     9001BOC107     9001BFB107
BR202 - BR214     9001BOC214     9001BFB214
BR215 - BR219     9001BOC218     9001BFB214


Schneider Electric Canada