{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What are the repair parts for the H362AWC, series F7 (may be shown as F07)?
Issue:
Repair parts

Product Line:
HD Safety Switch

Resolution:
The repair parts for the H362AWC, series F7 (F07) are as follows. No other parts are available.
-Line Base Assembly - 4056603850 (requires one. Arc Suppressor not included)
-Load Base Assembly - 4056604050 (requires one)
-Line and Load Base Mounting Screws - 4020515101 (3 for line, 2 for load)
-Arc Suppressor Assembly - 4056635550 (requires one) (Obsolete and replaced with part #NNZ51874 - requires One )
-Arc Suppressor Mounting Screw - 4020514501 (requires one)
-Lug Assembly - 4025101652 (per lug)
-Lug Mounting Screw - 4020514202 (per lug)
-Mechanism Assembly - 4056787350 (NOTE: also recommend replacing Switch Mechanism Gasket and Handle Gasket)
-Switch Mechanism Gasket - 4056786001
-Mechanism Washer - 2360200008
-Handle Assembly - 4056663550 (also recommend replacing Handle Gasket)
-Handle Gasket - 4056603101
-Lockplate - 4056672101
-Lockplate Mounting Screw - 2299940562 (2 required)
-Rod/Linkage Assembly - 4056787050
-Receptacle - 2541002311
-Receptacle Mounting Screws - 4510280101 (4 required)
-Ground Lug - 4025101652 (3 total required)
-Ground Lug Mounting Screw - 4020513503 (2 total required)
-Fuse Pullers ? FPK0610 (1 required)

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: