Issue:
Repair parts
Product Line:
QO Circuit Breaker Enclosure
Resolution:
The equipment ground kit, part number PKOGTA2, is the same for all the below QO circuit breaker enclosures:
QO2100BNF, QO2100BNS, QO2100BNRB, QO2125BNF, QO2125BNS, QO2125BNRB, QO3100BNF, QO3100BNS, and QO3100BNRB
NOTE: the PKOGTA2 is only a set of two tang lugs that will mount together in the enclosures, see visual below
Repair parts
Product Line:
QO Circuit Breaker Enclosure
Resolution:
The equipment ground kit, part number PKOGTA2, is the same for all the below QO circuit breaker enclosures:
QO2100BNF, QO2100BNS, QO2100BNRB, QO2125BNF, QO2125BNS, QO2125BNRB, QO3100BNF, QO3100BNS, and QO3100BNRB
NOTE: the PKOGTA2 is only a set of two tang lugs that will mount together in the enclosures, see visual below