{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can Circuit Breaker plug-in units be operated from the floor with a Hook Stick?
Issue:
Operate a Circuit Breaker plug-in unit from the floor with a Hook Stick

Product Line:
I Line circuit breaker plugs

Environment:
Products sold and used in North America

Resolution:
I Line plug-in units can be operated using the hook stick as a standard feature.
PowerBus225 plug-in units have this feature as an add on to the standard plug-in unit.

Schneider Electric Canada