{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can a Buck-Boost Transformer be utilized on a 50hz system, even though the nameplate shows the Transformer to be rated for 60Hz?
Issue:
Buck Boost Transformers used on 50 Hz systems

Product Line:
LV Transformers

Environment:
Applies to Low Voltage Transformers by SquareD/Schneider Electric

Cause:
50 Hz systems are used in many parts of the world

Resolution:
In some cases, yes.  If the induction levels of magnetic flux in the core of the Transformer resulting from the applied voltage at 50Hz do not exceed the unit`s acceptable induction levels, then it can be done.

Schneider Electric Canada