{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the replacement lock kit for an NQOD, NQO or NQOB NEMA type 1 panel trim?
Issue:
Replacement locks for an NQOD, NQO or NQOB NEMA 1 cover?

Product Line:
NQOD, NQO or NQOB panelboards

Environment:
Products sold in North America

Resolution:
NOTE:  All these panelboard families are obsolete.

All trims up to 50 inches and vented trims 53 inches to 68 inches if manufactured before 1/6/1997, use lock part number PK4FL  If after 1/6/1997 use the lock part number PK22FL.
All fronts on boxes 56 inches high or higher (excluding 53 inch through 68 inch high vented fronts) if manufactured before 11/01/1999 use lock part number PK5FL .  If after after 11-01-1999 use the PK22FL.
The lock kits includes 2 keys.
The replacement key only is part number is LP9618.

Schneider Electric Canada

Explore more
Category:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Category: