{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Are two pole QO-GFI breakers available with a 22K AIC rating?
Product Line:
Circuit Breakers
QO-GFI

Environment:
Electrical Distribution Equipment

Resolution:
No, 10,000 AIC is the only available rating for the two-pole GFI without using series ratings.

Schneider Electric Canada