{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Will an arc fault breaker work in an old house with a grounded 2 wire system with no ground wire?

Issue:
Do arc fault breakers work with circuits that do not have a ground?

Product Line:
Miniature Circuit Breakers

Resolution:
Yes, it will work as long as the circuit is grounded and it has a segregated neutral. Absence of a ground wire will not affect performance of the AFI or CAFI breaker.

Schneider Electric Canada