{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Are transient suppressors available for the F-line contactors?
Issue:
Identify the part number of the coil suppressor for TeSys F Contactors

Product Line:
Tesys F Line Contactors and Accessories

Environment:
IEC Contactors and Starters

Resolution:
Yes there are suppressors for coils up to 220 volts, 50/60 Hz. Select these based on control coil installed; standard control coils provided with devices ordered with coil codes are LX1 type.
Suppressor modules clip-on mount directly to control coil. For separate mount on 35 mm DIN rail or panel mount order bracket number LA9D09981.

For coils LX1FF, LX1FG & LX1FH use suppressor part number LA9F980.

For coils LX1FJ, LX1FK, LX1FL, LX1FX, LX9FF, LX9FG & LX9FH use suppressor part number LA9D09980.

Note: LC1F800 contactors are provided with coil suppression as standard.

Schneider Electric Canada