{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is the Form R6, two wire control relay, an option on a 8903 PB lighting contactor?
Issue:
Adding a 2 wire control relay option on an 8903 Panelboard lighting contactor

Product Line:
8903 Panelboard Lighting Contactors

Environment:
NEMA Contactors and Starters

Cause:
Would like to use 2 wire control for the PB lighting contactors

Resolution:
No, they do not come with an R6 form from the factory. However the customer can field-install an interposing relay.

Schneider Electric Canada

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.