{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What are the repair parts for an RC2M200S, series M01?
Issue:
Repair parts for RC2M200S Series M01.

Product Line:
CSED

Resolution:
NOTE: WIRING DIAGRAM AND LABELS ARE NOT INCLUDED ON THE PARTS LISTED BELOW.
The parts listed here are the only parts considered field repairable that are still available:
Meter Cover Assembly - 4056206950
Main Breaker Section Cover Assembly - 4053449250
Main Breaker Section Cover Hinges - (2) X2983
Main Breaker Section Cover Hinge Mounting Screws - (2) 2159414081
Dead Front Interior Trim Mounting Screw - 4020513001K (contains 10 screws; only 1 is required)
Dead Front Interior Trim Filler Plates - (2) QOFP
Meter Base Assembly - 4056250150 (includes meter base, (2) line side lugs, (4) meter jaws and meter jaw blade guides, (2) load side lugs (feeds QO base), and load side bussing (feeds QOM2-VH))
Meter Jaw - (4) 7329794850
Meter Jaw Mounting Nuts - (4) 2342702001
Meter Jaw Blade Guide - (4) 4052761901
Left Line Side Lug Assembly - 4056207850
Right Line Side Lug Assembly - 4056207950
Fifth Jaw Kit - 5J
Closing Cap - (2) ACP
Primary Main Breaker - QOM2-VH type, 200 A maximum
Main Breaker Mounting Nuts - (2) 2342702001
Secondary Main Breaker - QO-VH type, 50 A maximum
Main Breaker Mounting Base - 4050443650
Mounting Screw - 2196617201
NOTE: WIRING DIAGRAM AND LABELS ARE NOT INCLUDED ON THE PARTS LISTED ABOVE

Schneider Electric Canada

Explore more
Category:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Category: