{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What replaces the Q1 tenant breakers used in the old obsolete 100 A sockets for vertical and unitized EZ Stack, multi-metering devices?

Article available in these languages: Spanish

Issue:
Is there a suggested replacement for Q12100 breaker in the obsolete EZM or UEZM devices?

Product Line:
Residential metering equipment

Resolution:
The 100 A, vertical and unitized EZ Stack devices accepted either QO or Q1 tenant breakers, 2 pole, 15 - 100 A. QO breakers were used for requirements from 15 through 70 A (inclusive) and Q1 breakers were used for requirements for 70 through 100 A (inclusive). The Q1 breakers are obsolete and no longer available, but can be replaced by QO breakers.

Schneider Electric Canada

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.