{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
9007C54B2 - Does this include a lever arm?
Issue:
Is the lever arm included on part number 9007C54B2?

Product Line:
9007C Limit Switch

Environment:
NEMA Limit Switches

Resolution:
No, for selecting 9007 Type C lever arms see page  21-34 of Digest 177.

Schneider Electric Canada

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: