Search FAQs
What does the "R" (or "R-Handles" pointing to dash lines) printed on spaces on the old load center directory labels mean?
Issue:
Installation of Replacement Tandem Breakers in non-Class CTL load centers
Product Line:
Load Centers
Resolution:
That marking is an indication of spaces in which tandem breakers (Replacement Tandem Breakers only) are permitted to be installed in that load center. The "R-Handles" indicates the second handle circuit of an old style tandem breaker which was constructed with the handle throws above and below each other. These would then be on the left and right as the breaker was installed in the panel.
![](https://ckm-content.se.com/ckmContent/servlet/servlet.ImageServer?id=0151H000008zrrXQAQ&oid=00DA0000000abSm)
Note: these load centers can NOT accept QOT tandem circuit breakers. They only can accept the replacement tandem breakers for use in non-class CTL load centers found in the below table:
Installation of Replacement Tandem Breakers in non-Class CTL load centers
Product Line:
Load Centers
Resolution:
That marking is an indication of spaces in which tandem breakers (Replacement Tandem Breakers only) are permitted to be installed in that load center. The "R-Handles" indicates the second handle circuit of an old style tandem breaker which was constructed with the handle throws above and below each other. These would then be on the left and right as the breaker was installed in the panel.
Note: these load centers can NOT accept QOT tandem circuit breakers. They only can accept the replacement tandem breakers for use in non-class CTL load centers found in the below table:
Replacement Tandem Circuit Breakers
Ampere Rating[2] | Cat. No.[4] |
---|---|
1P—120/240 Vac—1 Space Required | |
15 A and 15 A | |
15 A and 20 A | |
20 A and 20 A | |
20 A and 30 A | |
30 A and 20 A | |
Two 1P Individual Trip—120/240 Vac—2 Spaces Required | |
15 A and 15 A | Order Two QO1515 or QO2020 circuit breakers and handle tie QOTHT |
15 A and 20 A | |
20 A and 20 A | — |
20 A and 30 A | |
30 A and 20 A | — |
[2] 10–30 A circuit breakers are suitable for use with 60oC or 75oC conductors. 35–125 A circuit breakers are suitable for use with 75oC conductors.
[4] UL Listed as HACR type for use with air conditioning, heating and refrigeration equipment having motor group combinations and marked for use with HACR type circuit breakers.
[11] Includes two circuit breakers (one QO2030 and one QO3020) and handle tie QOTHT.
Released for:Schneider Electric Canada
Explore more
Range:
Category:
Explore more
Range:
Category: