Issue:
Define QOUQ breaker
Product Line:
Miniature Circuit Breaker
Resolution:
It is a QOU breaker provided with four-point quick-connect terminals. This is a permanent factory installed terminal affixed to the load or OFF end of the breaker. This special terminal will accommodate up to four 1/4-inch female quick connect wire terminations.