{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What are the lug sizes for the ATS48D62Y, ATS48D75Y, ATS48D88Y or ATS48C11Y?
Issue:
Lug size for Altistart 48

Product Line:
Altistart 48  ATS48

Environment:
All

Cause:
N/A

Resolution:
The ground conductor is max of 4 AWG and Power Terminals are max of 2/0 AWG.
It is not necessary to provide lugs for this soft starter. The terminals are part of the unit.

Schneider Electric Canada