{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the separate mounting kit for the LRD** and LR3D** Tesys overload relays?

Article available in these languages: Spanish

Issue:
Separate mounting kit needed for a Tesys overload relay
** represent the two digit current adjustment range (i.e. LRD01, LRD02, ...LRD35 or LR3D01, LR3D02, ...LR3D35 )

Product Line:
IEC Contactors and Starters

Environment:
Tesys D overload relays

Cause:
separate mounting required for the application

Resolution:
Separate mounting kits for mounting to 35 mm DIN rail or for panel mounting with screws:

LAD7B10 (Not UL/CSA recognized)  for LRD01–35 and LR3D01–35
or LAD7B106 for LRD01–35 and LR3D01–35  with ring tongue terminals.

Schneider Electric Canada