{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What are the repair parts for a QOM22225NRB, Series S01 enclosed circuit breaker?
Issue:
Current Design repair parts

Product Line:
QO load centers

Resolution:
Only the parts listed below are considered field replaceable.
Outdoor Cover - 4056546350 (includes the Circuit Breaker Cover)
Circuit Breaker Cover - BCV
Base Assembly - 4055938950
Base Mounting hardware - 4020510001 (4 required)
Neutral Assembly - Included in base assembly
Neutral Bonding Screw - 4028345850K
Bag Assembly - 4028356350 (includes mounting screws and keps nuts)
NOTE 1: An interior dead front trim is not used in this device. Access to the operation of the circuit breaker handle is through the BCV cover.
NOTE 2: The BCV is mounted to the cover with rivets. The rivets used should be .125`` diameter with a recommended grip range of .126-.187. A bead of sealant is required to be applied around the base of the cover to maintain the NEMA 3R (rainproof) integrity. Dow Corning #731 Sealant, or equivalent, is recommended.
The rivets and sealant are not provided with the cover.

Schneider Electric Canada

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: