{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the difference between 9002AW7 and 9002AW12 foot switches?
Issue:
Need to know the contact difference of 9002AW7 with 9002AW12.

Product Line:
Push Buttons and Operator Interface

Environment:
9002A Heavy Duty Industrial

Resolution:
9002AW7 has a mechanical latch.  When you push the petal down the contacts latch until you manually unlatch them with the lever on the switch.  See page 7 of 65013-010-31H for the picture of the mechanical latch.  9002AW12 is a push on/push off maintained contact switch.  Also 9002AW7 has a single pole double throw contact whereas 9002AW12 has a single pole single throw contact.

Schneider Electric Canada